Other Parts Discussed in Thread: TPS3839
I have inherited a battery charger design from someone and am evaluating it. The design application does not have a practical access to an I2C buss for setting up the device. I want the device to be capable of running as follows:
1) Providing power from a bank of rechargeable Li-ion batteries to a load.
2) Accepting input from a USB source to charge the bank of rechargeable Li-ion batteries. Would like for the battery charge current to be 2A, which appears to be the default. It also appears that the input current limit from VBUS, which I believe would be the source of power to charge the batteries, is by the resistance between ILIM and ground, as the this is the default state for ENILIM.
Based on what I have learned so far, it does not appear that use of the I2C buss is required for my simple application. Is this correct?
I am also wondering if the original designer over specified in selecting this part, that is I wonder if a simpler part, with fewer supporting components, could be used in this same application. Actually when I look at the schematic it is pretty simple already, but I thought it did not hurt to ask.