This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am using TPS54531 for an out put of 5V,5A. My input is 6V to 7.4V. I am using a battery as input. My battery cut off voltage is 6V. So I need to disable the IC when input falls below 6V. So what will be the values of Ren1 and Ren2. I cannot understand what is Vstart and Vstop for my design. So please help me with it.