Dear support member.
My customer consider the LM25061 for using jig at the time of assembly at the factory.
I have a question.
<Conditions>
A hot swap controller is not mounted on the system side.
A hot swap controller is only mounted on the jig side.
<Question>
Q1
Will it work even if a LM25061 controller is mounted on the jig side (≠ power supply side)?
Q2
I want to connect in the order of ①GND ⇒ ②power supply ⇒ ③signal line in the jig side circuit.
Can it be realized with this LM25061?
Q3
GND and the order of power supply can not be guaranteed.
Does such a configuration work as designed?
Best regard.
Bob Lee.