This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2595: [TPS259573] Hot Short to GND

Part Number: TPS2595

Hello, I want some advice to e-fuse device.

Use the following power specifications.

1. Design e-fuse circuit to Datasheet reference

2. Input Power : 14.4[V] / 2~3[A]

3. e-Fuse Setting I-Limit : 1.3[A]

4. e-Fuse Setting Over Voltage : 15[V]

and then, i'm doing short-circuit test to output and ground. 3-4 times is okay, but after that it is broken.

Does anybody know why an e-fuse is broken? I need advice on this situation.

thanks