Part Number: BQ20Z95
Hi,
We currently are working on a "old" product that we have to maintain and support.
The current cells are not available anymore so our customer selected a new cell for us to assemble the pack.
Since it is a new Cell I started with the cycles for the ChemID and got stuck at reconfiguring the bq20z95.
My Problem is that the old cell had way less capacity in comparison to the new one. Our Customer does not want a significant increase in capacity for reasons unknown to us and he will most likely not drop this Requirement.
The whole Gas Gauging Algorithm used by bq20z95 depends on the Chemical depth of discharge and the total chemical capacity Qmax. Therefore, as I understand we have to set the chemical Qmax for the new Cell with a Golden Cycle that will Result in the real chemical capacity the Cell has so that the ChemID and OCV-Tables as well as the Gauging in its entirety will still work.
Further i think we can increase the DF:Terminate Voltage and DF:Reserve Capacity to Reflect the FCC we actually want. As an Example
with a 3000mAh Standard Cell with 30% at 3.6V we would have a FCC of 2100 as long as we set the DF:TerminationVoltage to 3.6V
and the DF:ReserveCapacity to 900mAh. This way we could still use the "usual determined" ChemID and the OCV-Tables would also not
disrupt anything as long as we stay above the 3.6V. Is this Assumption correct?
I was reading the "SLUA364 - Theory and Implementation of Impedance Track". It is not clear for me if the DOD1 and DOD2 used at
the new "TerminationVoltage" would Result in a Qmax of 2100 when the previous settings in the example are used and if there would
be any weird behavior in the GasGauging itself.
Can u tell me if the simple parameterchange proposed and a Golden Cycle with these Settings as well as the ChemID i got from Cycling the
Cell (min/max values specified in the Datsheet) would give us the Outcome our Customer wants or if we have to approach this from a different angle ?
Thanks in advance
Robert Andris