This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51200DRC pin equiavalent device for 2v5 output

Used this device on a design for 2v5 output from 3v3 input. Now aware chip is limited to max 1v8. Is there a pin equivalent or nearest part that can go to 2v5 output from 3v3 input? Not using the REFOUT & PGOOD pins. Device is enabled all the time. Current output capacity between 0.5 to 1 A range is acceptable.