This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2373: replace Opto-isolators for TPH, TPL and BT by TI Isolator

Part Number: TPS2373
Other Parts Discussed in Thread: ISO7730

Dear team,

Because my customer have to use the TPL/TPH/BT 3 pins indicator which are isolate signals. I saw datasheet suggest to use Opto-isolators, may I know could we use TI Isolation solution like ISO7730 to replace? If yes, may I know if there is any 5V from TPS2373 primary side that could be used to power ISO7730? Because maximum Vcc1 of ISO7730 is 5.5V. Thank you.

Regards,

Polly Chung

  • Hi Polly,

    You can derive 5V from either the 48V Vdd or the 12V VC_In (from the bias winding). This can be done with an LDO or resistor divider and a 5.1V zener diode connected between the Vcc1 of the ISO7730 and RTN.

    Best,
    Tom