A customer has an unusual request:
For various motor brakes they need an 8A output with adjustable voltage in the range of 12V-48V, though those precise voltages are not set in stone. Preferably 1V steps.
The input is 24V +/- 20%, so about 19V-29V range.
Something like this: http://www.ti.com/lit/an/slva251/slva251.pdf - but of course with much higher output voltage/current.
I would simply do it, but I am worried about the compensation network not changing, as well as how hard it will be to EMC test. I'm thinking fixed-frequency would be preferable.
Does TI have a recommended solution, or just suggestions, for this application?