This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS548A20: THe maximu uty cycle of TPS548A20 and TPS549A20

Part Number: TPS548A20
Other Parts Discussed in Thread: TPS549A20

Hi

My customer will use TPS548A20 or TPS549A20 under Vin=5V and Vout=3.3V.
Could I use those devices under this condition?
Could you tell me the max Duty cycle of TPS548A20 and TPS549A20?

Best regards,
Yokota
  • Yokota-san,
    There is no direct limitation to duty cycle. The maximum duty cycle is determined by the minimum off time ( 240 nsec typ, 310 nsec max) and teh selected switching frequency. So for your case, the maximum switching frequency = (1 - (3.3 / 5)) /310E-9 = 1.098 MHz. You should be able to use any of the switching frequency options of 850 kHz or lower.