This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC24612: Can we add a gate driver UCC27517 to work together with UCC24612-2 ?

Part Number: UCC24612
Other Parts Discussed in Thread: UCC27517,

Hi 

Our application is LLC with 4.25V / 50~60A output.

Can we add a gate driver UCC27517 to work together with UCC24612-2 for this application?

or is there any other suggestion? 

Thanks!

PY Tsai

  • Do you mean you want to insert UCC27517 between UCC24612 and MOSFET? UCC24612 works to regulate MOSFET VDS with VG voltage. If UCC27517 is between UCC24612 and MOSFET, VG won't regulate MOSFET VDS. Can you draw a circuit to show how you want to connect UCC27517 in your proposal?

    To make other suggestions, can you provide your LLC secondary side circuit configuration, how many MOSFETs in parallel etc?