Hello.
I have a question about the OCP 3 threshold of UCC 256302.
Variation of the threshold of OCP 3 is shown in the data sheet
Temperature -40 ℃ to 125 ℃: 0.49V to 0.79V.
How is the variation of -10 ℃ to 125 ℃?
Also, what is the variation at 25℃ ambient temperature?
typ: 0.64 V = 25 ° C is good? Is there a variation?
Thank you.