This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24600: Can this IC be used to charge 6cell 7.4V, 10AH battery

Part Number: BQ24600

Hi team,

I am  designing a charger circuit for 7.4V, 10Ah battery with 6 number of cell , So I am planning to use BQ24600 IC .

My concern is that the maximum charge current of my battery is 5A and the adapter input voltage is 9V DC supply now I m bit confused like how to configure the charging IC according to my application ,Please can anyone provide me a circuit for my application.What resistor configuration should I keep? Please support its first time i am dealing with battery operated device.

Regards,

Karthik