Hi team
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team
Ricardo san,
I tested it with a circuit made of breadboard.
And I will send new measurements with no problem device.
In this case, there was no problem with reset operation, but the waveform of WDI periodically outputs pulses. Is this the problem behavior?
This time, in the device which is a problem, it instantaneously falls to low as the pulse of this WDI like the waveform sent yesterday.
Best regards
Hayashi
Hayashi san,
1. You mention the first scope and second scope capture are same circuit but different device. Is WDI left open in either scope capture? Is the WDI signal the same for each circuit?
2. If the WDI works as normal, the /RESET should wait for delay time upon return. You are correct. It looks like the delay is very short since the time scale on the scope capture is 5us / division. Is this correct? The /RESET should remain low for approximately 200ms. Is anything else connected to /RESET pin?
3. I would like to know how many devices you have tested, and if the issue occurs everytime? Can you also try to reduce the VDD capacitor to 0.1uF?
-Michael
Hayashi san,
Because the /RESET is such a short delay, this could be a defect. I would like to know the result when decreasing the capacitor. When the WDI pin is floating, the watchdog disables and the scope capture should be similar every time.
Do you have another device you can try to see if it is defected device or problem with your application or circuit board?
-Michael