Hi,
one of my customer is testing the BQ21040 battery charger IC & is using the schematic from the datasheet application note .
the battery detection is proper & we are getting 3.6V o/p when battery is connected .
But the indication LED is not turning ON .
also , i am getting around 1.4V at the cathode of LED .
Please help in addressing the issue .
REgards
mandar