This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1H100-Q1: Maximum Current-limit value by RCL

Part Number: TPS1H100-Q1

Hi,

We got a question from the customer about TPS1H100-Q1.
Could you help us?

[Question]
How much is the recommended maximum current limit value which the IC can set the +/-14% accuracy by RCL? dKCL/KCL is defined +/-14% at Ilimit>=1.6A, but there is not maximum Ilimit condition.

Best Regards,
tateo

  • Hello,

    The current limit accuracy is better with higher current limit. The device has 2 current limits, internal and external ajusted by extrnal pull down resistor Rcl. The internal current limit lower limit is 7A. The external current limit is guaranteed up to 7A. The 14% accuracy is guaranteed up to 7A by external Rcl. 

    Regards