We bring up BUCK3 @ 3V3 second last (BUCK1 @ 1V0 is last) and occasionally this rail fails to start up. What happens is that the 5V Point-of-Load supply that feeds BUCK3 drops out due to over-current.
The first thing we suspected was too much distributed capacitance on the 3V3 rail – in a detailed audit of local decoupling and reservoir capacitors we found in excess of 400uF. Removing most of this did not produce any change in behaviour.
On a hunch we decided to disable the BUCK3 discharge resistance and this caused the issue to vanish. The question is why? The default value is BUCK3_DISCHG[1:0] = 0b01 for a 100Ω load. This should equate to only 33mA maximum! The 5V PoL is designed for 5A – 25W and we should have ample headroom given the total dissipation of the unit is under half that figure.
Wonder if anyone could shed any more light on this.
Thanks,
Dave.