I implemented BQ25896 as charger and power line for kind of mobile tracking device. Everything works fine according to power line but have weird registry problem.
I'd like to read battery voltage during battery operation. I set REG02 bit 6 and 7 to 1 to turn on ADC and 1s readings.
When I read REG05 while VBUS is connected to external power adapter, everything works fine.
But when I disconnect VBUS and working on battery only the register shows all zero bits which is actually not true.