Part Number: UCD3138
Hello,
I have the following questions about UCD3138HSFBEVM code and appreciate urgent help:
1- In " handle_vout_prebias_state" function" , how is the scaler voltage is calculated for input (30) and output(6)? What is 0.101 and 9.901?
2- In " handle_vout_prebias_state" function" , how is the scaler from ADC to DAC (6.15) is calculated?
3- In " handle_idle_state" function" , how the DAC_VALUE for the current and voltage is calculated ? I mean why 11800 stands for 12A and 7000 stands for 40V?
4- In " configure_ovp " function in configuration_functions.c, what does 5.12 stand for? How is this number calculated?
5- In " configure_iout_ocp " function in configuration_functions.c, how is 2.414 calculated?
I really appreciate detailed responses to these questions and not just referring to the user guide.
Thanks,