Hello
Please find my schematic attached to this post.
We are trying to develop a 3-cell Li-ion charger with this part. There are quite some issues that are present.
1. With a Vref = 3.3V , the voltages with the dividers at ISET, ACSET should be 0.8V, but I measure as 0.65V (all resistors are 1% and accurate)
2. I have set the CELL/FB at 10V (for checking) but with a resistor load i get around 7V or lesser still. Yesterday I got 4V there. With a capacitive load I get similar voltages.
3. STAT is constantly blinking on resistive load, but i believe that is bound to happen. Since the chip is expecting a battery connected at the output.
4. With a 3-cell battery connected at the output and a 16V/10A source(fixed voltage and current) there was no limit to current, all 10A was flowing in the battery. I immediately shut off input power to prevent further damage.
5. If i limit the input current to 2A, there is around 100mA current flow in to the battery.
6. I am not using the System output anywhere, I just need the battery output, which is going on to another cell balancing part ISL94203 (Currently it is not connected)
What is the problem? Please advise