This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55010: TPS55010

Part Number: TPS55010


Hi Anthony,

We test add a 3K ohm resistor (See attached schematic of R658)on the output as we discussed before to keep the voltage about 5.5V.

But output voltage still keep in 6.5V with 3K ohm resistor when no load on the output.

The output will reduce to 5V when add a 33 ohm resistor.

But 33 ohm draw too much power and TPS55010.pdfthat is not a solution.

Do you have any idea about how to reduce the voltage ?

Thanks!

Chin