Hi all,
When test the Transient performance of TPS51620, The output Vcore and Phase looks abnormal.
CH1 is Phase, CH3 is Vcore.
Do you have suggestion to debug it? Any material you want to have ? Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
When test the Transient performance of TPS51620, The output Vcore and Phase looks abnormal.
CH1 is Phase, CH3 is Vcore.
Do you have suggestion to debug it? Any material you want to have ? Thanks
Thanks Carmen,
That is not used for intel core. It was used for Zhaoxin core. The test was done by the DC eLoad. Do you have any comments on such kind test? such as the slew rate or any setting need to be done during this kind of test?
I am trying to get the sch now.
Hi Cheng,
Since we've moved to email to resolve the issue I'm going to close this thread.
Cheers,
Carmen