Dear, support team.
The absolute maximum rating of the LM4040 has no regulation of the power supply voltage.
"8.2.2.2 Cathode and Load Currents" in the data sheet description.
"At the other extreme, maximum VS and minimum IL, RS must be large enough to limit IZ to less than its maximum-rated value of 15 mA."
Is the power supply voltage unlimited if it is within 15 mA as RS setting?
Please advise me about the supply voltage.
Best Regards,
Hiroaki Yuyama