Hi Expert,
NRES & ENDRV have internal pull up resistor. Which internal power rail does these pull-up are connected? What is the voltage for the pull-up power rail?
Thanks.
Zhou
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Expert,
NRES & ENDRV have internal pull up resistor. Which internal power rail does these pull-up are connected? What is the voltage for the pull-up power rail?
Thanks.
Zhou
Hi Zhou,
Please refer to figure 5-14. Reset and Enable Circuit, the pullup and circuit paths for NRES and ENDRV pins VDDIO (IO supply input) is shown. The VDDIO supply voltage normally tied to VDD3/5 which is the rail from the device assumed to be used for the IO supply in the system. VDD3/5 is configurable for either 3.3V or 5V operation.
Best Regards,
Scott