To whom it may concern,
I use the LT1054IP to convert +12V to -12V. The +12V/-12V are used for the power of the OP amplifier. I measure the current in the -12V circuit, the current is 14mA . Sometimes the LT1054 will fail, the voltage will be 0.X V. I think that the output current of LT1054 is sufficient for my load current(14mA). Can you give me some advice? The attached file is my circuit. Thank you.