This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS56121: Differebce BTW TPS56121 AND TPS56121B

Part Number: TPS56121


Hello, Team,

I found there was TPS56121B on the web.

What is the difference BTW original TPS56121 and TPS56121B?

What are the changes from original part?

Best regards,

Hidekazu Someno

  • Hi Hidekazu,

    We will try to find that information for you

    Thanks
    -Arief
  • Hidekazu,

    Some of the changes are listed below...
    EN/SS functionality: After soft-start is complete, the EN/SS pin is changed to EN pin (soft-start multiplexed functionality is removed). This prevents negative inductor currents in case of slow pull-down of EN_SS pin during shut-down.
    Gate-drivers/PWM: Gate driver logic changed to avoid shoot-through in the case of PWM double-pulsing. PWM circuit modified to avoid double-pulsing.
    Thermal shutdown fault: The TSD fault is now digitally filtered and latched.
    Besides these the input voltage abs max changed from 14V to 16V and Abs max ratings for SW pin was added.

    Regards,
    Mathew