This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: Current measure min Unit 1mA or 10mA or ?? when 30A .

Part Number: BQ34Z100-G1

Hi 

I have very simple question for Current measure for  Min Current Unit. 

We thinking measure current  until 30A ,  Yes this is very high Current .

[ Question  ] 

   What is min current unit  when  30A current measure  ??

   Yes , we want to know  measure current resolution .

   1mA  or 10mA  or ???? 

Sorry ... very simple question.

Regard

March Jasper  (  Sugimoto  in Japan ) 

 

  • Hi March Jasper,

    The device reports values in 1 mA increments. The deadband value will need to change as you change the value of your current sense resistor. The voltage drop across the current sense resistor should not exceed +/-125 mV.

    Sincerely,
    Bryan Kahler