This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A85: Request for a product (TPS7A85)

Part Number: TPS7A85


To whom it may concern,

I have a question about TPS7A85.

The datasheet stated that the output voltage range of the regulator is 0~5V.

However, the output voltage of up to 6V seems to be also possible if the input supply voltage set to 6.5V and the external resisters set well (for example, R1=12.4Kohm, R2=1.9Kohm).

Excuse me, could you let me know whether the TPS7A85 can supports an output voltage of 6V ?

I am looking for a regulator with an output voltage of 6V and an output current of more than 4A.

Thank you very much in advance.

Sincerely,

Jongwon Lee.

----------------------------------------------

KAIST Institute for IT Convergence, Senior engeneer

E-mail: temuchin80@kaist.ac.kr

Tel: 82-10-5577-3449, 82-42-350-4294

  • Hi Jongwon,

    TPS7A85 was designed, characterized, and tested for output voltages up to 5 V.  

    We do have a few linear regulators that are designed for higher output voltages and rated for more than 4 A.  You can find these regulators on our parametric search.  I have filled out the Vout and Iout requirements on the parametric search for you here.

    Very Respectfully,

    Ryan