This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR23625: Maximum soft start time

Part Number: LMR23625

Hi team,

I'm an FAE supporting some industrial company at Japan.

My customer have question about internal soft start time.

Its datasheet shows soft start time is 2ms(NOM) and 6ms(NOM) at HSOIC package and WSON package respectively.

Could you please provide MAX soft start time for each package?

The soft start time after enabling must be within 10ms for the customer's application.

Following is peripheral info of LMR23625 at customer's application.

  • Load : FPGA(Intel/MAX10) 
  • Output Voltage: 3.3V

I'm looking forward to hearing back from you.

Best regards,

Shota Mago