This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63061: Vin rating compared to number of cells to be used

Part Number: TPS63061


Dear Team

The following question came from our partner:

We are using in our design TPS63061 in a system with up to 8 batteries. Can you clarify why it is stated in a datasheet that it is intended for three-cell up to six-cell batteries if the input voltage is up to 12V (which would in theory allow eight 1.5V alkaline cells).

Kind regards
Gabor