This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5069: LM5069

Part Number: LM5069


Hi, our system is powered by 48V battery and we use LM5069 as in-rush current controller. The external circuit is designed as the datasheet and the parameters are as below:

Rsns=2mΩ;

Rpwr=22k;

Ctimer=0.1uF;

Cout=3000uF;

Q1:STP100N10F7: 100V/80A

The maximum bus current is 30A and the problem is Q1 is easily burnt at the moment of power on.

Your reply are highly appreciated.