Dear Specialists,
My customer is considering TPS23753 to the their system and has an inquiry.
I would be grateful if you could advise.
---
We are currently considering to install in our products, we are making a study useing in Class 4 at the point of maximum power consumption.However, since the minimum power consumption is about 9 W, it does not match the PD Class 4 range (12.95 - 25.5 W) in the table above. If the power consumption deviates from the class 4 power range, what will happen? Please tell me about both cases where it falls below or exceeds the power range.
---
I appreciate your great help in advance.
Best regards,
Shinichi