Other Parts Discussed in Thread: TPS40140,
Hi team
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team
Hayashi-san,
1. As explained in datasheet, 15mV or larger ripple voltage promises smooth transition between CCM and DCM.
I think this restriction is from the accuracy of TPS51116 current sense amplifier.
2. When external sensing resistor is used, the current sense is not related to Rds(on), therefore there is no restriction for low Rds(on).
3. If CC2 is used, CC2 and Rc together will create a pole and this pole can be used to cancel the zero from Cout and its ESR.
The ceramic cap ESR is very small, the zero from Cout and its ESR is at high frequency region. Usually this zero will not affect cross frequency and phase margin. Therefore CC2 is not needed if ceramic cap is used.
Electrolytic cap ESR is larger. If the zero from Cout and its is at very low frequency region. It is an option to use CC2 to create a pole to cancel ESR zero.
It is not saying CC2 must be used. It is just an option.
For your design, I would suggest to keep a placeholder for CC2 and set it "not populated" in BOM. So you have choice to use CC2 or not based on test result.
Thanks
Qian