Hi Team,
Iq and Packages
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Eggsy,
I would recommend looking at our TPS7A05 which is also available in a 1x1 mm package. Looking at both datasheets it seems both devices are rated for Iq from a minimum 0.6uA. However it seems that our TPS7A05 has a higher PSRR and a lower dropout rating.
GPN | XC6504 | TPS7A05 |
AEC Q100 | NO | NO |
Output Options | Fixed Output | Fixed Output |
Iout (Max) (A) | 0.15 | 0.2 |
Vin (Max) (V) | 5.5 | 5.5 |
Vin (Min) (V) | 1.4 | 1.4 |
Vout (Max) (V) | 5 | 3.3 |
Vout (Min) (V) | 1 | 0.8 |
Fixed Output Options (V) | 1.1 to 5 | 0.8, 1.0, 1.2, 1.5, 1.8, 2.5, 2.85, 3.3 |
Enable | YES | YES |
Power Good | NO | NO |
Output Capacitor Type | Ceramic | Ceramic |
PSRR @ 100KHz (dB) | 5 | 15.4 |
Noise (uVrms) | N/A | 227 |
Accuracy (%) | 1 | 1.5 |
Vdo (Typ) (mV) | 260 | 204 |
Iq (Min) (uA) | 0.6 | 0.6 |
Hi Jose,
Thanks for your help! Customers feedback they would like to try them.
Another question, Customers would like to use two LDO in their board and if we have two channel LDO with low Iq and small package which they prefer.
Do we have two channels LDO with low Iq and small package?
Thanks!