This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53353: Ripple injection

Part Number: TPS53353


I have two DC/DC converters based on TPS53353. They both work set to 3,6V, both are identical, same components.

No I am wondering why the ramp(lower picture) which I inject to the VFB pin is a little different in one converter, they both are around 50mV. 

Question is why: one sawtooth is let say  not  "ideal"? 

They are both with noise and spikes I see but why the ramp is not continuous, we can observe a big drop around the peak.
I reduced the amplitude even to 30mV, so that's not the reason. The first picture is with a good Ramp