This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC256303: Fullbridge LLC pri. wire low side 2xMOSFETs drive <ISO Driver>

Part Number: UCC256303
Other Parts Discussed in Thread: UCC5310,

Hi all,

I want to configure the Full Bridge LLC by using one UCC256303.

How to connect to drive pri.wire low side 2x MOSFETs?

In case of using two Iso Gate Drivers UCC5310, how about below.

For high side mosfet drive trans connection :  Rvcc-Vcc1, GND to GND1, LO to IN+   and  Vcc2- Drain, Vout and CLAMP- Gate, VEE2- Source(SW node)

For low side mosfet drive trans connection : HB-Vcc1, HS to GND1, HO to IN+   and  Vcc2- Drain, Vout and CLAMP- Gate, VEE2- Source(GND)

Is this OK ?  Any additional caution point?