This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have the TPS92512 set up almost identical to the set up created by web bench except that
1. I and enabling the unit via 0-5v pulse into PDIM. For the purpose of trouble shooting this is currently a constant 5v as soon as the micro powers up.
2. I have a thermistor set up to scale back the power if the board gets too hot.
Note: the system drives 3 parallel paths of 2 creee XQE LEDs
When I turn on the system I get a quick blip as shown below, the scope grab is measured from ground to pin 7 and is thus a current measurement. It appears for the first 20ms that the chip is stuck at 100% duty cycle and allowing for 5.6A of current, after that start up glitch it works properly limiting to about 0.3v at pin 7. The glitch happens almost every boot cycle but varies in duration. Do you have any thoughts on what may be causing this?
that's odd i had two images a schematic and a scope grab that showed up when i posted.
Vin on my test is 15vdc
Vled measured 6.9vdc
ILED = 0.475A normally and 1.25A when it's in the goofy over current glitch. ( 3 paths of leds to triple those numbers for total current)
The micro has control after 5.6mS
If my post works there will be screen grabs below of the the current glitch, Comp pin in figure 2, De featured Schematic Figure 3. I added a pull down resistor on the PWM pin to control it before the micro boots up. This appears to fix the problem. So the micro before boot is tri stated, and the converter has a weak pull up so that means the converter is trying to turn on; but has a open on the output as none of the LED paths are enabled so no current should flow at that point. Once the micro boots the converter and one LED path is enabled, this is where the high current occurs until some system on the converter goes back to normal.
Figure 1: Input spike in current and normal current measured across a 0.41 ohm resistor in series with a LED path.
Figure 2: yellow input system current across a 0.1 ohm resistor. Pink V comp pin.
Figure 3: