Hi team,
I'm an FAE supporting some industrial companies.
My customer is considering using BQ25890 so that it can be used with a certain load in the case of w/o a battery.
Specifically, he considers current of VSYS to be 3.5A or so.
Then, he provided 3 questions as follows
- Regarding Fig.5, is this battery chargeable condition(CHG_CONFIG=Enable and CE_=LO)?
- Could you please provide the data of VSYS load regulation when increasing the VSYS w/o battery?
- Just for making sure understanding
In terms of Fig.6, since VBAT is 4.2V, it means charging is nearly compete and it's almost supplied to the SYS side.
Is this correct?
I'm looking forward to hearing back from you.
Best regards,
Shota Mago