This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS659037: Crystal frequency tolerance

Part Number: TPS659037

Dear Specialists,

My customer is evaluating TPS6590378 and has question.

I would be grateful if you could advise.

---

I have a question about the oscillator (16.384 MHz) for TPS6590378.

When I measured the OSC 16 MIN frequency using the oscilloscope's frequency counter function, the value is about 16.382 MHz (@ room temperature).

It is not within ± 30 ppm of the device specification.

In this case, how will it affect the operation of the device?

For reference, I measured it even with the EVM of AM 5726, but since it was the same result here, it does not seem to be a problem peculiar to this board.

---

I appreciate your great help in advance.

Best regards,

Shinichi