This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ29700EVM-610: BQ25101 + BQ29700 circuit design

Part Number: BQ29700EVM-610

Hello TI team

I have new battery part number RJD3048 charging and protection circuit design. Please attach files for schematic and battery. My battery charger design is for fast charging at 40mA. The average output current is around 4.4mA and peak current is around 350mA.  Could you please help to check if my design is suitable for this battery? 

Also, is the battery able to be charging when battery is below cutoff min battery voltage?

Thank

Best rgds

Bon  battery charging Schematic.pdfRJD_Series_Rev2016_battery.pdf