This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TPS54061: Output of TPS54061 is not stable

Part Number: TPS54061


Tool/software: WEBENCH® Design Tools

Hi Tis,

My ctm use TPS54061 as their buck DC/DC, Input is 12V ,output is 5V /200mA. At beginning provide 12V input, the Output is 5V,but it lasted a short time, it  went down to 0V。But when after a while, it could become normal output. the sch is as follow. Would you give some advice for the issue?