Part Number: LM25116
Other Parts Discussed in Thread: CSD19533Q5A, CSD16322Q5
Dear everyone,
For a project I have to do during my apprenticeship, I need to design a power supply able to deliver a maximum of 10A with an output of 26 or 15V. I chose the LM25116 because it seemed to be adapted.
However, I haven't been able to make it function correctly for now, despite having a schematic issued from WEBENCH tool.
The main problem I have on my design is the MOSFETs driving signals. They are not nice squarish waveform but damped oscillating signals (for Vgs) which conduct to have noise on my output voltage, even with no load.
Can anyone help me one this one ? I can provide the original schematics as well as the modified version I have done while testing. If needed, I can also provide some useful Gerber files because I suspect my routing to be part of the problem.
Thank you by advance,
Florian
(PS: please correct any speaking mistakes I could do. I am French so learning English is an every day challenge for me)