This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV1117LV: 4.5Vin/3.3Vout/1A application

Part Number: TLV1117LV

Hi Team,

 

Sorry to bother you.

I would like to use TLV1117LV to support 4.5Vin/3.3Vout/1A application. Can this LDO support this condition?

Thanks a lot.

 

Yours Faithfully

Redick Lee

  • Hi Redick,

    heat dissipation will 1.2W then. Junction to ambient thermal resistance is 63°C/W, resulting in temperature rise of 76°C over ambient. So, with an ambient temperature of 40°C junction temperature will be 116°C. Hhm, this is quite a bit, isn't it? Can become critical if the cooling is nonideal or the ambient temperature is even higher than 40°C. Is the 1A load current drawn all the time or only temporarily?

    Kai