Hi Support team,
My customer found a reference design PMP5652 using TPS92210, but their output current needs to be doubled of PMP5652. Is TPS92210 still applicable for their design? Here is the spec requirements:
- Input voltage: 200-440Vac
- Output voltage: 100-150Vdc
- Ouptut current: 500mA to 700mA
- Efficiency requirment: 90% @ 230Vac (at full load)
- PF requirement: 0.98 @ 230Vac, 0.93 @ 480Vac,
- THD: THD<20% with load ≧ 50% at 230/347Vac input
- Dimming: 0~10V analog dimming
Or please suggest better solution for the listed spec.
Thank you.
Best Regards,
Wei-Hao