Part Number: BQ25071
Other Parts Discussed in Thread: BQ24650,
Hello,
We are evaluating using either the BQ25071 or BQ24650 for Solar Charging a LiFePO4 battery: The questions are related to the BQ25071. We see that the BQ25071 is simpler and optimized for LiFePO4, however does not have the VDPM explicitly called out in specs unlike the BQ24650. Here's our Solar and Battery Specs:
Solar Panel: I sc=165mA; Vosc=4.8v; Vmppt=4v; Imppt=150mA
Battery:
- A 1550 mAh LiFePO4
- Nominal Voltage of 3.2v
- Charging voltage of 3.65+/- 0.05v
We will have the ISET limit set to 150mA by choosing the 1.5Kohm Resistor value.
It's all well and good under good sunlight conditions with power generated at 150mA/4v, however under non optimal solar irridance conditions we will have a much lower power generated.
Assuming that we will have current let's say in the 50mA range and the voltage Vin into BQ25071 meets all the other minimum conditions (VULO < Vin and Vin > VBAT + VSLP):
Would this low current be able to charge the battery? (example condition of lets say voltage of 3.9V and Current of 50mA and VBAT at 3.5v)?
If not, what are the minimum current requirements? We would like to get the charging trickle as much as we can as the device will be outdoors for most of the day.
Does the current limit setting of 150mA affect the 50mA charging?
If you have any Appnotes/pointers on the usage of BQ25071 for solar harvesting, please let us know.
Thanks,
Krishna