HI,
My Question is very specific to READ_TEMPERATURE_1 (8Dh) register . Based on the valued of m ,b and R for this register. It simply reduces to the Y/16 . Where Y = A 2-byte two's complement integer received from device.
But on page 28 . It says the range of this register is 0000h-0FFFh to indicate -256C to 255C . If the range of Y = 0000 to 0FFFh that means the MSB is never set then how are the negative temperature values represented ??
So the details in the data sheet corresponding to this register are not so clear, more info on this would be highly appreciated