This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27421-G1: bq27421-G1B battery chemistry

Part Number: BQ27421-G1
Other Parts Discussed in Thread: BQ35100, GPCCHEM
 We're using the bq27421-G1B fuel gauge IC. 

The older version of the bq27421-G1 technical reference (SLUUAC5, June, 2013) states:

• bq27421-G1A is pre-defined for LiCoO2 -based batteries for 4.2 V max charge voltage.
• bq27421-G1B is pre-defined for LiMn2O4 -based batteries for 4.3V or 4.35V max charge voltages
The revised version SLUUAC5C (Aug, 2016) states:
• The bq27421-G1A fuel gauge is predefined for LiCoO2-based batteries for 4.2-V maximum charge voltage.
• The bq27421-G1B fuel gauge is predefined for LiCoO2-based batteries for 4.3-V or 4.35-V maximum charge voltage.
• The bq27421-G1D fuel gauge is predefined for LiCoO2-based batteries for 4.35-V or 4.4-V maximum charge voltage.
We're using an IMR (LiMn2O4) battery with the bq27421-G1B fuel gauge. Is the bq27421-G1B accurate enough to gauge the LiMn2O4 batteries?