This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM846C23: Current share for more than three phase

Guru 19655 points
Part Number: TPSM846C23
Other Parts Discussed in Thread: TPSM846C24, , PTH08T250W

Can TPSM846C23 or TPSM846C24 use current share for three phase or more?

I looking for power module for large current solution; 12Vin ⇒ 0.85Vout / 90A

When multi current share is not recommended, is there any solution for power module?

Best regards,

Satoshi

  • The TPSM846C23 or C24 can only current share up to 2 devices for up to 70A.

    PTH08T250W can be paralleled for higher current that would meet your application requirements

    We also have several power module devices in development capable of delivering higher current. Please contact me directly at jarrigo@ti.com for more information.