TPS543C20 has PGND, GND and AGND pins.
How should we separate these GND?
I think VSEL, SS, RT, MODE, RAMP and ILIM pin resistor GND should be connected to AGND pattern and BP and VDD capacitor should be connected GND pin. Then GND pin and PGND is connected on inner layer.
Finally, AGND, PGND and GND should be connected at thermal PAD point as a one point GND connection.
However I think these GND connection are not separated definitely on EVM pattern.
GND of VSEL resistor etc... are connected GND pin pattern on the Top layer. And those are connected to GND pattern of Inner Layer 1.
Is not the way of these GND connection so severe?
Is it better to separate definitely?
Best Regards,
Kohei Sasaki