Hello
We see data sheet page1 is 0.01%(10,000:1) for PWM dimming range.
So, Customer is evaluating TPS92518 EVM.
Customer applies PWM signal from their MCU to TPS92518EVM.
Customer's issue is ILED =0 mA at PWM=0.1% duty. ..test result is excel file.
Customer is using CREE's 36V/1A LED. (VIN=48V)
Anyway,
I had tested TPS92518EVM myself using PWM signal in LEDSPIMCUEVM and GUI, using same CREE's LED,VIN=48V.
I had also found that ILED is approx 0mA at PWM=0.1% duty.
My test result is attached PPT.
Q1
Customer's and my test result about ILED was approx 0mA when duty = 0.1% ... but would you please advise about the reason?
We want to know whether our usage ( register setting ) was wrong or no.
Q2
We see TPS92518 EVM user's guide (sluubm0) Fig4 shows Output current 5mA~10mA even duty=0%.
We want to know how to add Offset as Fig4 of user's guide.
( I heard from you that Fig4 is based on PWM dimming only ( not shuntFET dimming) , but how do you achieve Fig4 ?)
Q2
We think the corrective aciton should be customer's MCU set higher duty in case small duty ,intentionally.
But concern is linearity curve ( gain/offset) may be changed each VLED ( Customer will use several kind of VLED in their same PCB).
Do you think linearity curve ( gain/offset) may be changed by VLED ?
( I should ask customer to use 0x0Ah~ 0x0Fh for VLED reading?...)
Thank you for your support!
Thank you for your cooperation
Best Regards