Hello.
I have a question about UCC256302.
About the system external stop function
① About restoring from external system shutdown
⇒ When we confirmed the waveform, we started it after entering FAULT.
From the data sheet Figure 44, it does not apply to the condition to enter FAULT, and it does not understand the factor of entering FAULT.
② About operation in external stop
⇒ Data Sheet If you check with the operation in Figure 44, I think that it will shift to LIGHT_LOAD_RUN at the moment of short circuit and shift to 13 after 200 ms.
Assuming that the input voltage of LLC is sufficiently high and assuming BLKstart = 1, it shifts from JFET OFF to 3 → 4 and stays in WAKEUP (because it does not apply to the transition conditions of 4, 11, 15, 19).
Since it can shift to 11 when the voltage of Vcc becomes 10.7 V or less with the passage of time, it shifts to JFET ON.
Is it okay to recognize that you are repeating this situation?
(If the input voltage of LLC is low and BLKstart = 1 does not hold, I think I will stay at JFET OFF) b
For details, please check the attached document.
Thank you.20180714_質問 (1).xlsx